Saving energy, conserving resources and ensuring a sustainable supply chain - this is what we do in the Planet field of action.
Innovative products and processes
We see two perspectives for more sustainability here: on the one hand, the focus is on our products and services themselves, which enable lightweight construction, downsizing of components and material savings, for example. On the other hand, the Planet area is also about developing measures to ensure that our products can be manufactured more sustainably. In terms of content, these range from the use of renewable energies to the optimization of processes in order to minimize waste.
Sustainable joinings for industries of the future
Our products are already helping to reduce weight and emissions in many industries - or create stable connections for industries of the future, such as the production of renewable energies.
Generating high-strength threads in plastic e-car charging plugs - with AMTEC® thread inserts
Reinforcing threads in wind turbines, for example in the generator area - with HELICOIL® thread inserts
Creating load-bearing threads in thin-walled sheet metal for fastening photovoltaic modules - with RIVKLE® blind rivet nuts
Optimization potential in joining technology
Sustainability is commonly associated with terms such as "durable", "environmentally friendly", "resource-saving" and "reusable". All of these properties also apply without restriction to one of the most commonly used fasteners: the screw.
Screws are produced in a highly economical cold forming process. Only a small amount of energy is required in the production process, while hardly any raw material is lost. Loosening and reusing a screw is also possible without any problems - provided that the connection is suitably designed. This means that not only can an already assembled component be detached and reused, repaired or professionally recycled. The screw itself can also be easily returned to the recycling loop at the end of its service life.
In practice, the optimal design of connections offers additional potential. However, the performance of fasteners is often not used efficiently enough. One reason for this is that technical developments are constantly creating new requirements for joining and fastening technology that are impossible for designers to keep track of.
This is where we come in with our ECOTECH application technology consulting service. An experienced team of technicians and engineers advises and supports our customers in designing connections that are as efficient as possible - and therefore ultimately more sustainable. This is because functional optimization often ensures that an equally stable connection is created with fewer different and smaller dimensioned connecting elements than before - and therefore less material and use of resources.
Smaller component dimensions and weight savings can also be achieved in this way. A benefit for our customers as well as for the environment.
Optimizing Böllhoff System (OBS)
The Optimizing Böllhoff System (OBS) plays a fundamental role in our company when it comes to the sustainable and responsible use of resources. The basic idea of OBS is to create value without waste.
OBS pursues the goal of optimally coordinating all activities that are necessary for value creation through process optimization and thus avoiding superfluous activities (waste). To achieve this, existing processes must be viewed from two perspectives, scrutinized and continuously improved:
From the perspective of the customer, whose wishes regarding availability, individuality, quality and pricing of a product must be fulfilled in the best possible way.
From the perspective of our company, which must always operate profitably and improve its competitiveness.
What does OBS do?
This question can be answered with the four basic OBS principles:
Climate change poses major challenges for the entire world population.
The continuous rise in the global average temperature can only be stopped if we all do our part. It is therefore part of our corporate responsibility to make a contribution to environmental and climate protection and to continuously take further steps towards carbon neutrality. To this end, we analyse the emissions that we cause directly and indirectly, identify potential and initiate measures to reduce emissions.
Energy
Some Böllhoff Group sites have had a certified energy management system in accordance with ISO 50001 since 2015. This standard has established itself as an international standard since its publication. A key component of energy management is the detailed recording of energy flows and energy sources within the company. Only if these parameters are known can potential savings be identified and realized. The focus is always on reducing energy consumption by increasing energy efficiency.
At Böllhoff, we rely on the modernization of control technology and data acquisition systems. Both help us to continuously evaluate the energy balance of our production facilities, buildings and logistics processes - and to optimize them in the long term. The aim of the energy management system is to systematically record and evaluate our resource flows and derive suitable measures to continuously improve efficiency.
Facts, figures and data
By looking at our energy consumption in detail, both in relation to emissions and in relation to our turnover, we can see how energy-intensive our business activities are. Viewed over a period of years, this allows us to derive a global trend in our group of companies. This shows us whether our measures in the areas of energy and emissions are taking effect.
*This is provisional data, which is partly based on previous year's figures, as the actual data is not yet available.
**This is a sales office where the energy consumption is included in the rent and is not shown separately. Therefore, the consumption is constantly estimated.
The past few years have clearly shown us the importance of a secure and price-stable energy supply: In the Böllhoff Group, process optimizations for energy-intensive areas in production are therefore particularly relevant.
Clearly defined and ambitious savings targets are just as important as the involvement of management and intensive communication.
An important step towards greater energy efficiency is to obtain a precise overview of all consumption. Thanks to the continuous expansion of our data collection, energy consumption can now be precisely determined in a large proportion of all production areas.
Using various key figures, we are able to identify specific optimization potential - and reduce the relative energy consumption per production and logistics unit.
There are individual energy saving targets here: For example, the companies with certified energy management systems have the target of reducing energy consumption per million parts produced by 1.5% per year.
The commitment of the energy and environmental managers on site is also crucial: they carry out numerous projects at the locations in order to achieve the respective energy targets.
Measures
In order to drive forward specific measures for energy savings, we look at two dimensions within the company: our infrastructure on the one hand and our processes on the other.
As we are a manufacturing company, many potential savings can already be achieved in the area of infrastructure. Among other things, we look at building equipment, ensure efficient lighting and ventilation in our buildings and keep our machinery up to date.
One example: In recent years, we have successively replaced our hydraulic plastic injection molding machines at the Bielefeld production site with all-electric models wherever possible. Due to their design, all-electric models are much more energy-efficient than hydraulic ones.
In addition, we delve deep into processes to identify further optimization approaches. Even small adjustments often lead to major improvements, especially in production processes. Among other things, we look at the optimization of machine parameters and the standby and ramp-up times of our machines.
Use of renewable energies on the rise
Photovoltaic expansion at Böllhoff
To use every technically suitable roof in Germany to produce solar power by 2025 - and also commission more systems internationally: This is the target we have set ourselves. High time for an interim report.
"Driving continuous improvement within the company: We also pursue this goal when it comes to energy. As our employees know all the processes best, it is crucial to involve them - and to create an awareness of savings among them. We achieve this through regular training and workshops."
»
Emissions
We attach great importance to transparency and regular reporting when presenting and disclosing our emissions. We have therefore committed to carrying out our accounting in accordance with the guidelines of the GHG Protocol (Greenhouse Gas) and the SBTi (Science Based Targets Initiative).
In doing so, we rely on an approach that aims to avoid emissions first, then reduce them and finally offset them. From the end of 2024, we will also have our balance sheet audited externally to ensure the highest standards.
Our focus is on reducing emissions along the entire value chain in order to make a sustainable contribution to environmental protection.
Facts, figures and data
In terms of emissions, we consider both the emissions in our own business division (Scope 1 and 2) and in our upstream and downstream value chain (Scope 3) - in each case in relation to our turnover. The corresponding emissions figures reflect the fact that the majority of emissions are generated within our value chain. This results in major reduction potential for the future, always in close coordination with partners such as suppliers and customers.
2023 [t CO2e]
2022 [t CO2e]
2021 [t CO2e]
Change on previous year [%]
Change compared to base year 2021 [%]
Scope 1
5,824*
5,490
6,092
6
-4
Scope 2
9,709
9,129
13,367
6
-27
Total Scope 1 and 2
15,533*
14,619
19,459
6
-20
Scope 3
391,104
395,729
390,438
-1
0
Total Scope 1–3
406,637
410,348
409,897
-1
-1
*This is preliminary data, which is partly based on the previous year's figures, as the actual data is not yet available.
With our participation in the Science Based Targets Initiative, we are also setting ourselves specific targets for the reduction of Scope 3 emissions - i.e. emissions from our value chain - for the first time from 2024.
In Scope 1 and 2 - i.e. our direct emissions and indirect emissions from purchased energy - we are aiming to reduce greenhouse gas emissions by 25% by the end of 2024 (compared to the base year 2021). We have also set ourselves the goal of being CO₂-neutral in Scope 1 and 2 by 2030.
Measures
In order to achieve our emissions targets, our reduction measures must be implemented at various levels.
Energy management plays a key role in Scope 1 and 2. Here, we can reduce emissions by increasing efficiency and expanding and using more renewable energies.
However, our focus is on Scope 3 - i.e. in our upstream and downstream value chain - particularly with regard to purchased goods and services. This is where we want to identify and implement appropriate savings measures through our participation in the Science Based Targets Initiative.
Apprentices develop savings potential
Energy scouts at Böllhoff
We also actively involve our apprentices in our endeavours towards sustainability - by making them energy scouts, together with the Bielefeld and Detmold Chambers of Industry and Commerce. This is because apprentices often develop the most exciting ideas for savings thanks to their uninfluenced view of operational processes.
At Böllhoff, we are committed to protecting the natural foundations of life. We minimize unnecessary environmental impacts and reduce unavoidable ones. Our priority is the careful use of natural resources throughout the entire product life cycle - from development, energy consumption and production to use and subsequent disposal.
Our annual environmental program serves to define, evaluate, review and certify our goals.
Use of resources
The careful use of all natural resources is important to us. At the same time, as a manufacturing company, we have an increased need for resources in the production of our goods. Bringing these two poles together in the best possible way is one of our key challenges on the road to a more sustainable future.
In order to optimize our use of resources, we therefore pay particular attention to the raw materials used for our products. When it comes to resources, this is where we have the greatest leverage to make our fasteners more sustainable. We are therefore increasingly using recycled raw materials wherever this makes ecological and economic sense. In view of climate change, we are also focusing more on the issue of water management within the company.
Materials used
2023
2022
2021
Semi-finished products for production:
Rods [tonnes]
4,076
4,305
4,108
Wire [tonnes]
12,972
12,992
12,838
Granulate [tonnes]
1,538
1,621
1,895
Trade goods from:
Rods [tonnes]
27,971
40,132
29,891
Steel [tonnes]
3,334
3,810
4,077
Plastic [tonnes]
270
421
473
Aluminium [tonnes]
160
191
165
Brass [tonnes]
35
99
45
Copper [tonnes]
358
382
350
Recycling at a glance
In our plastics technology, recycled granulates are also used to produce fasteners; in metal production, the proportion of recycled brass fasteners is around 75%.
The proportion of recycled steel scrap in our trade goods made from various steels is around 40%.
Water
The relevance of water management is increasing, even in our latitudes. Due to climate change, dry and hot summers are no longer an exception. As a result, water is becoming increasingly scarce in many countries - with phases of better and worse availability throughout the year. This results in growing demands on water management.
Although water as a resource is not used intensively in our business model, we are addressing the issue. This is already being done at the first locations where treatment makes sense.
In future, we want to take a closer look at the topic of water management at company level and back it up with overarching targets and measures. The first step is to make water withdrawals at our sites around the world transparent.
2023
2022
2021
Change on previous year [%]
Change compared to base year 2021 [%]
Total water withdrawal [m³]
47,278
42,068
44,846
12.4
5.4
Water withdrawal per employee [m³]
14.8
13.2
14.9
11.8
-0.9
Locations in water stress areas*
5 locations in China, Spain, Turkey, India, Mexico
*Evaluation using Aqueduct Water Risk Atlas, classification "Extremely High"
Facts, figures and data on waste
In addition to steel and non-ferrous metals, we also use a variety of different plastics to manufacture our own fasteners. The unavoidable metal and plastic waste from sprues, missing parts and other rejects generated during production is a valuable resource. The recycling of these materials is our top priority and is part of our comprehensive waste concept. This concept enables us to collect all metal and plastic waste from production by type and then recycle it.
In this way, we aim to achieve a recycling rate of 100% for these recyclable materials. For example, some of the recovered raw materials are ground up directly on site and fed back into production as regranulate.
2023
2022
2021
Amount of waste
Total [tonnes]
4,933
5,059
4,727
Non-hazardous waste
Of which thermally disposed [tonnes]
350
367
333
Of which recycled [tonnes]
4,451
4,597
4,296
Hazardous waste
Total [tonnes]
1,845
1,681
1,051
Total amount of waste [tonnes]
6,778
6,740
5,778
Recycling share
66%
68%
74%
Supplier management and sustainable supply chain
Just as we live sustainability within the company ourselves, we also expect our suppliers to act responsibly. To ensure a sustainable supply chain, we therefore work closely and in partnership with all suppliers. On the one hand, we look at how our partners implement sustainability in their own company, for example with regard to energy and emissions. On the other hand, we also look at how they fulfil their corporate social responsibility.
Due to our business distribution, the core areas in our procurement process are Germany, Europe and Turkey. Smaller quantities are also sourced from East Asia. In countries where there is an increased risk of human rights violations, suppliers are monitored very closely: through on-site visits and numerous audits. Böllhoff does not tolerate any kind of violation of human rights by suppliers and will block the supplier.
Our Code of Conduct is an important tool for ensuring a sustainable supply chain. It is part of the general terms and conditions of purchase and contains important topics relating to corporate social responsibility.
Procurement: global or local
In principle, we are interested in global competition. However, for ecological reasons, we attach particular importance to procuring materials locally whenever this is possible and makes economic sense. This prevents long transport routes that are associated with additional emissions.
In today's globalised world, we understand local procurement to mean that goods or services are procured at a national level - i.e. they do not have to cross national borders on their way to the respective Böllhoff site.
The following table shows the percentage of the procurement budget that is spent on suppliers located close to the respective Böllhoff site:
2023
2022
2021
Change on previous year [%]
Change compared to base year 2021 [%]
Total share
56.5%
50.0%
54.6%
6.6
2.0
Sustainability projects worldwide
Creating more sustainable joinings - with recycled steel
Countless joining elements are made from steel every day. This is also the case at Böllhoff. In France, we rely on recycled steel as a raw material - 100 per cent from 2025.