Success stories
An avoidable cost factor: fast wearing threads. With our biggest-ever HELICOIL® thread inserts we were able to extend the service life of the tools.
Initial situation
When manufacturing large pipes, the company uses a two-head expander in the final forming stage.
The welded pipes are gradually cold-enlarged using the expander to achieve the dimensional accuracy and the required geometrical data. The expansion rate differs depending on the pipe’s diameter, the thickness of its walls and the material used. It varies between 0.8 % and 1.5 %. The permanent strain of up to 1,500 tonnes of tensile load caused wear to the threads on the expander's tension rods. Due to the resulting costs, a long-lasting solution was needed.
Solution
Heavy loads call for strong solutions. We worked together with EUROPIPE to develop an tailor-made solution. This involves screwing a HELICOIL® thread insert into the tension rod nut to improve distribution of the pre-tensioning force during the mechanical expansion process. Increasing the thread’s fatigue strength significantly extends the service life of the mechanical expander.
For EUROPIPE, we have produced our largest HELICOIL® thread inserts ever, measuring:
204 x 16 x 282 mm, 260 x 20 x 330 mm and 320 x 25 x 420 mm.
Result
We work closely with our customers to develop tailor-made solutions. This is just one example of that close collaboration.
With HELICOIL® inserts we created wear-resistant, high-precision threads. Increasing the strength of the threads made it possible to extend the service life of the expander tension rods.
Customer benefits
we will be happy to help.
Just let us know and we’ll get in touch
Contact us