Search
Country and language
Choose country:
Choose language:
Apply
  1. Böllhoff Thailand
  2. News from the Böllhoff Group
  3. Böllhoff Group receives ISO 19443 certification

23/08/2024 | Company

Böllhoff Group receives ISO 19443 certification

Certification to ISO 19443 strengthens the Böllhoff Group's position as an innovative manufacturer of fastening solutions for the civil nuclear industry.

Böllhoff Group receives ISO 19443 certification

ISO 19443

ISO 19443 is an internationally recognised quality standard that was developed specifically for companies in the nuclear industry supply chain. It extends the requirements of ISO 9001 to include specific requirements for nuclear safety and quality.

We are pleased to announce our successful certification according to ISO 19443

Certification to ISO 19443 strengthens the Böllhoff Group's position as an innovative manufacturer of fastening solutions for the civil nuclear industry. Our HELICOIL® thread inserts, which are used in the nuclear industry to reinforce and repair threads, are particularly worthy of mention here. Our HELICOIL® thread inserts are particularly suitable for applications with high safety and quality requirements, which are common in the nuclear industry.

The certification enables us to become more competitive internationally and to expand our activities in a highly regulated market. 

Our production plant for thread technology plays a central role here. Not only the HELICOIL® is manufactured here, but also a wide range of other products that meet the highest quality and safety standards.

We are one of the few companies in the world to fulfil the strict requirements of ISO 19443. This certification demonstrates our commitment to the highest quality and safety standards and underlines our ability to meet the demanding requirements of the nuclear industry.

This might also interest you